Question, i.MX8M Quad Lite clock inputs

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question, i.MX8M Quad Lite clock inputs

2,334 次查看
SLICE
Contributor IV

Dear team,

I would like to ask about the clock inputs to i.MX8M QL.

All of 25MHz, 27MHz and 32.768KHz input are required for i.MX8M?

The customer will not use HDMI, and they want to remove the 27MHz. And they want to use divided clock from 25MHz for 32.768kHz if accuracy is not needed.

Regards,

Miyamoto

标签 (1)
0 项奖励
回复
5 回复数

2,186 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

>The customer will not use HDMI, and they want to remove the 27MHz.

it is ok, as for clocks 25MHz and 32.768KHz they are required for i.MX8M, please also check

Boot without external RTC 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,184 次查看
SLICE
Contributor IV

Hello Igor,

Thanks for your support.

https://community.nxp.com/message/1010000?commentID=1010000#comment-1010000?q=i.MX8M%20clock%20input

And HDMI_REFCLK_P/N can be left open when HDMI is not used.

And 27M crystal cannot be removed even if user does not use HDMI.

Correct?

Regards,

Miyamoto

0 项奖励
回复

2,184 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

HDMI_REFCLK_P/N can be left open when HDMI is not used according to

Table 30 – i.MX8M Unused Signal Strapping Recommendations i.MX8M User Guide

Best regards
igor

0 项奖励
回复

2,184 次查看
SLICE
Contributor IV

Hi igorpadykov

Thanks a lot!

As for the each of clocks, are there any requirement such like deviation or jitter?

Regards,

Miyamoto

0 项奖励
回复

2,184 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

for clock requirements please check i.MX8M Hardware Developer’s Guide
https://www.nxp.com/docs/en/user-guide/IMX8MDQLQHDG.pdf

Best regards
igor

0 项奖励
回复