Question, i.MX7D TEST_MODE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX7D TEST_MODE

1,963 Views
Aemj
Contributor IV

Dear team,

I would like to ask about TEST_MODE input pin of i.MX7D.

In i.MX7 hardware development guide(IMX7DSHDG, Rev.0), it is mentioned as below.

“The TEST_MODE input is internally connected to an on-chip pulldown device. The user must tie this signal to GND.”

On the other hand, TEST_MODE pin is externally pulled-down through 100K ohm register on i.MX7-SABRE board.

Could you show me which is correct?

Actually, my customer made their own i.MX7D board. And they saw clock oscillation did not work when they add the 100K ohm pull-down register. And after removing the 100K ohm, the oscillation worked.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
4 Replies

1,855 Views
Yuri
NXP Employee
NXP Employee

Hello

 

  The TEST_MODE pin should be pulled down. The problem in Your case

may be concerned with noisy environment, that requires more strong

pulling down. Please try 10 KOhm instead of 100 KOhm for it.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,855 Views
Aemj
Contributor IV

Hi Yuri,

Thanks for your prompt reply.

Can I understand that it is better for TEST_MODE pin of i.MX7D to be pulled-down via 100K-10K ohm register rather than direct connection to GND?

Thanks,

Miyamoto

0 Kudos
Reply

1,855 Views
Yuri
NXP Employee
NXP Employee

The TEST_MODE may be connected to GND directly.

~Yuri.

0 Kudos
Reply

1,855 Views
Aemj
Contributor IV

Hi Yuri,

I understand that the direct connection to GND and pull-down are both allowed.

Thanks,

Miyamoto

0 Kudos
Reply