Question, i.MX6UL BENAND

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6UL BENAND

3,016件の閲覧回数
Aemj
Contributor IV

Dear team,

My customer want to use the following Toshiba/BENAND chip with i.MX6UltraLite.

TC58BVG0S3HTAI0(BENAND)

Could you check whether the BENAND chip can be used with i.MX6UL?

Please find the attached file for the datasheet of the BENAND.

And please find the another attached file, the BENAND has a restriction on its programming.

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,860件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   TC58BVG0S3HTAI0 has embedded ECC, and  I am afraid, it is practically impossible to use "smart"

NAND with on-die ECC enabled for boot, since i.MX6 GPMI controller is intended to work with "raw"

parts, assuming specific NAND blocks mapping : any NAND is treated as sequence of 512-bytes blocks

with following spare areas. The ''smart' NANDs use own (different) mapping.

    Please look at section 8.5.2.5 (Bad Block Handling in the ROM) of the I.MX6UL RM (IMX6ULRM,

Rev. 0, 08/2015) for NAND data mapping. As for ECC - section 8.5.2.2 [NAND Flash Boot Flow and Boot

Control Blocks  (BCB)] describes BCB structures and states about ECC protection, using the internal

hardware.

   Possible solution – my opinion – applying boot SPI NOR; so that NOR code configures

BENAND part to disable its ECC (if possible).


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,860件の閲覧回数
Aemj
Contributor IV

Hi Yuri,

Thanks for your comment.

After boot-up, is it possible to disable ECC function on i.MX6UL by clearing GPMI_ECCCTRL[ENABLE_ECC] bit?

What do you think about the use as storage device, not for boot device?

Thanks,

Miyamoto

0 件の賞賛
返信

2,860件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hi,

   I am afraid, it is impossible to use the NAND as a storage device with its internal ECC.

The reason concerns specific NAND layout, used by GPMI, where 512-byte blocks are located

with the following spare areas (just after data block). This does not meet layout of the BENAND

part; as result ECC area of BENAND is mixed with data, expected by the GPMI.

  
     But it would be possible to use the BENAND part if its internal ECC is disabled.

Regards,

Yuri.

0 件の賞賛
返信