Question, i.MX6SoloLite start-up

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question, i.MX6SoloLite start-up

1,234 次查看
Aemj
Contributor IV

Dear team,

My customer is developing their board with i.MX6SoloLite, and they are facing the issue about start-up.

What they want to is;

- Using switch connected to ONOFF pin of i.MX6.

- When the first time VDD_SNVS_IN has been fed, PMIC_ON_REQ stays in L.

- When the switch is pushed -> PMIC_ON_REQ outputs H -> PMIC start the power-on sequence.

Against the above, the actual behavior is as below.

When the first time VDD_SNVS_IN had been fed -> PMIC_ON_REQ outputs H -> PMIC starts the power-on sequence.

I think the above behavior is the specification of i.MX6SL, but

Do you have any ideas to realize the customer’s requirement?

Thanks,

Miyamoto

标签 (1)
0 项奖励
回复
1 回复

1,117 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  Let me look at the scheme. You may send it via case 00073117.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复