Question, i.MX6SoloLite start-up

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6SoloLite start-up

1,223件の閲覧回数
Aemj
Contributor IV

Dear team,

My customer is developing their board with i.MX6SoloLite, and they are facing the issue about start-up.

What they want to is;

- Using switch connected to ONOFF pin of i.MX6.

- When the first time VDD_SNVS_IN has been fed, PMIC_ON_REQ stays in L.

- When the switch is pushed -> PMIC_ON_REQ outputs H -> PMIC start the power-on sequence.

Against the above, the actual behavior is as below.

When the first time VDD_SNVS_IN had been fed -> PMIC_ON_REQ outputs H -> PMIC starts the power-on sequence.

I think the above behavior is the specification of i.MX6SL, but

Do you have any ideas to realize the customer’s requirement?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 返信

1,106件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  Let me look at the scheme. You may send it via case 00073117.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信