Question, i.MX6SoloLite power-on sequence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX6SoloLite power-on sequence

1,081 Views
Aemj
Contributor IV

Dear team,

I would like to ask about power-on sequence of i.MX6SL.

Are there any restriction on the order of rising of VDD_HIGH_IN and NVCC_1V8?

My customer thinks as below.

VDD_HIGH_IN and NVCC_1V8 should rise during POR=L, and there is no matter whether the order of the rises is VDD_HIGH_IN, NVCC_1V8 or vice versa.

Is it true?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Reply

1,024 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

>VDD_HIGH_IN and NVCC_1V8 should rise during POR=L, and there is no matter

>whether the order of the rises is VDD_HIGH_IN, NVCC_1V8 or vice versa.

this is right based on datasheet requirements, however to avoid possible power supply

glitches during power-up it is recommended first to power-up VDD_HIGH_IN as it

controls internal power regulators circuitry.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply