Question, i.MX6SoloLite EVK/Android touch screen support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6SoloLite EVK/Android touch screen support

ソリューションへジャンプ
2,747件の閲覧回数
Aemj
Contributor IV

Hi All,

I would like to ask about the feature of android BSP(JB4.3_1.1.0) on i.MX6 SoloLite EVK.

In Android Release Note attached in your android bsp(JB4.3_1.1.0), it is said that UI input is not supported on i.MX6SoloLite EVK.

When using MCIMX28LCD with i.MX6SoloLite EVK, doesn’t the touch screen work with your AndroidBSP?

Could you show me how I can do for the touch screen to work?

BR,

Miyamoto

ラベル(2)
0 件の賞賛
返信
1 解決策
2,397件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Hi Miyamoto,

The touch panel on MCIMX28LCD does not work in i.MX6SoloLite EVK. You have to plug a USB mouse to the USB host port of the i.MX6SoloLite EVK to enable the user input.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,398件の閲覧回数
PeterChan
NXP Employee
NXP Employee

Hi Miyamoto,

The touch panel on MCIMX28LCD does not work in i.MX6SoloLite EVK. You have to plug a USB mouse to the USB host port of the i.MX6SoloLite EVK to enable the user input.

0 件の賞賛
返信
2,397件の閲覧回数
Aemj
Contributor IV

Hi,

Does anyone know how to make it work?

0 件の賞賛
返信