Question, i.MX6Q LinuxBSP LVDS setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6Q LinuxBSP LVDS setting

2,821件の閲覧回数
Aemj
Contributor IV

Hi All,

I would like to ask about LVDS display setting on LinuxBSP.

My customer is developing his i.MX6Q board with 640x480 LCD connected via LVDS.

Please find the attached file for the timing specification of the LCD.

He is developing his software based on your LinuxBSP.

He tried some LCD settings written in ldb.c as follows but could not make the LCD work.

Could you give your advice on what setting he should use for the LCD?

For struct fb_videomode;

{ NULL, 60, 640, 480, 39722, 48, 16, 33, 10, 96, 2, 0, FB_VMODE_NONINTERLACED, 0, },// cea_mode

{ NULL, 60, 640, 480, 39682, 48, 16, 33, 10, 96, 2, 0, FB_VMODE_NONINTERLACED, FB_MODE_IS_VESA },   // DVI setting

{ NULL, 72, 640, 480, 31746, 128, 24, 29, 9, 40, 2, 0, FB_VMODE_NONINTERLACED, FB_MODE_IS_VESA },

{ NULL, 75, 640, 480, 31746, 120, 16, 16, 01, 64, 3, 0, FB_VMODE_NONINTERLACED, FB_MODE_IS_VESA },

{ NULL, 85, 640, 480, 27777, 80, 56, 25, 01, 56, 3, 0, FB_VMODE_NONINTERLACED, FB_MODE_IS_VESA },


BR,

Miyamoto

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,360件の閲覧回数
YixingKong
Senior Contributor IV

Japan FAE

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel free to reply with an update to this discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,360件の閲覧回数
Aemj
Contributor IV

Dear All,

Sorry for my poor explanation.

The parameter entities listed in the previous post were added into 'static struct fb_videomode ldb_modedb[]' table in ldb.c.

Could you show me which of the parameters may suite for the LCD?

Please let me know if you need more information.

0 件の賞賛
返信

2,360件の閲覧回数
YixingKong
Senior Contributor IV

Japan FAE

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 件の賞賛
返信

2,360件の閲覧回数
Alvin
NXP Employee
NXP Employee

Hi,

Attached provides detail about display configurations on i.mx35. This method also apply to i.mx6.

Good luck! :smileyhappy:

regards,

Zheng Songhao

0 件の賞賛
返信