Question, i.MX6 SDMA/ loading script fails

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX6 SDMA/ loading script fails

1,201件の閲覧回数
Aemj
Contributor IV

Hi all,

I would like to ask about SDMA initialization.

My customer is trying to use SDMA with Freescale i.MX6 SDK.

The issue is;

Loading script fails in the initialization process for SDMA.

The sdma_load_init_script() function in sdma.c, which is included in your SDK, returns FALSE.

He found the SDMA_FLAGS_BUSY bit in sdma_envp->chan0BD.mode was not cleared and then returned FALSE at the line#99 in sdma_load_init_script().

This phenomenon means “Done” bit in buffer descriptor keeps 1 after completion of transfer, right?

According to the description in Table-55-49 in i.MX6DQ reference manual, D=1 indicates the SDMA has not yet processed in the case of channel 0.

Do you have any ideas about the cause of this issue?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

936件の閲覧回数
Aemj
Contributor IV

Hi All,

I am still waiting someone's response.

If anyone have a supplemental document which can be helpful for better understanding about SDMA handling, please provide!

BR,

Miyamoto

0 件の賞賛
返信

936件の閲覧回数
karina_valencia
NXP Apps Support
NXP Apps Support

Employee

Hi James,

     I have no source code in SDK, so I'm not sure whether SDMA_FLAGS_BUSY means "DONE"=1. Yes, it's abnormal if "DONE" always keep 1, which means SDMA NOT finish transfer or there is some error. But I suppose your BD setting are ok. No any SDMA transfer complete successfully or only someone?

0 件の賞賛
返信