Question, i.MX53 LVDS clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX53 LVDS clock

1,102 Views
Aemj
Contributor IV

Dear team,

I would like to ask about LVDS output clock of i.MX53.

When LVDS of i.MX53 is used as two output channels, can the output clocks of both channels be different?

If yes, please let me know which part of i.MX53, registers, should be configured to make different clocks for dual LVDS out.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Reply

1,015 Views
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

>When LVDS of i.MX53 is used as two output channels, can the output clocks of both channels be different?

yes

>please let me know which part of i.MX53, registers, should be configured to make different clocks for dual LVDS out.

please check description of IOMUXC_GPR2, Table 47-4. Channel Mapping  i.MX53 RM

and obds code examples in ../ipu/lvds_out.c

Lab and Test Software (2)
On-Board Diagnostic Suit for the i.MX53 Quick Start Board (REV 2011.39)
http://www.nxp.com/products/power-management/pmics/pmics-for-i.mx-processors/i.mx53-quick-start-boar...

May be useful i.MX53 System Development User’s Guide

http://www.freescale.com/files/32bit/doc/user_guide/MX53UG.pdf

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply