imx6slevk uboot bootargs spi_nor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

imx6slevk uboot bootargs spi_nor

2,172 次查看
威杨
Contributor III

Hello,

   i use imx6slevk,evk board has 4 M spi_nor,i want use it to boot the kernel . uboot bootargs about spi_nor's partition  is: mtdparts=spi32766.0:768k(uboot),8k(env),128k(dtb),-(kernel) refer to i.mx_Linux_User's Guide 24 page.i want to use 8M spi_nor,but i don't know spi32766.0 parameter how to set,could you give me some advises or give me some documents.

Thanks.

标签 (1)
0 项奖励
回复
1 回复

1,969 次查看
igorpadykov
NXP Employee
NXP Employee

Hi wei

please check attached Porting Guide

Chapter 5 Configuring the SPI NOR Flash Memory

and add support (if necessary) to this new spi-nor part.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复