Question, i.MX28 RTC backup

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX28 RTC backup

ソリューションへジャンプ
1,697件の閲覧回数
Aemj
Contributor IV

Hi team,

I would like to ask about RTC backup of i.MX28.

In i.MX28 reference manual, it is said as below.

“The RTC can continue to count time as long as a voltage is applied to the BATT pin…”

And i.MX28 datasheet says that BATT and the minimum voltage of DCDC_BATT pins is 3.1V.

I read the following discussion in i.MX community but please let me clarify about that again.

https://community.freescale.com/thread/307350

Can I understand that BATT and DCDC_BATT pins have to be fed 3.1V at least for keeping internal RTC alive?

If any other concerns, please let me know.

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,572件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

for keeping RTC sufficient only voltage applied to the BATT pin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,573件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Miyamoto

for keeping RTC sufficient only voltage applied to the BATT pin.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信