Question, i.MX28 PWD_OFF bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX28 PWD_OFF bit

1,201 Views
Aemj
Contributor IV

Dear team,

I would like to ask about PWD_OFF bit in HW_POWER_RESET register of i.MX28.

My customer saw that PWD_OFF bit field of i.MX28 could be 1 or 0 after u-boot was boot-up on their custom board.

That is, PWD_OFF bit seems not to be stable after uboot started.

In my understanding, the PWD_OFF bit is not affected by any hardware status.

The PWD_OFF bit is changed only by writing the register by software.

Is it true?

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Reply

1,135 Views
art
NXP Employee
NXP Employee

Q. The PWD_OFF bit is changed only by writing the register by software. Is it true?

A. Yes, this is true.


Have a great day,
Artur

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply