Question, i.MX28 EMI/ additive latency

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX28 EMI/ additive latency

ソリューションへジャンプ
1,785件の閲覧回数
Aemj
Contributor IV

Dear team,

I would like to ask about i.MCX28 EMI/ additive latency.

In i.MX28 reference manual, it is said the EMI does not support ‘additive latency’.

In my understanding,

If one needs to add additive latency, then one has to add the additive latency into CASLAT and also WRLAT parameter.

Am I correct?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,673件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Additive latency  (in the JEDEC Specification) allows a read or write command to be issued
immediately following the active command. In this sense we cannot  "add the additive latency"

for i.MX28.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,674件の閲覧回数
Yuri
NXP Employee
NXP Employee

   Additive latency  (in the JEDEC Specification) allows a read or write command to be issued
immediately following the active command. In this sense we cannot  "add the additive latency"

for i.MX28.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信