Question, i.MX233 power supply

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, i.MX233 power supply

ソリューションへジャンプ
1,715件の閲覧回数
Aemj
Contributor IV

Hi team,

I would like to ask about power supply feature of i.MX233.

Could you show me the settings for using internal linear regulator outputs of i.MX233 and stopping internal DCDC outputs?

In my customer’s understanding, to stop DCDC output;

- ENABLE_DCDC bit should be cleared.

To use internal linear regulators;

- 5V should be present.

- ENABLE_LINREG bit should be set.

To adjust offset voltage of the linear regulator output;

- set LINREG_OFFSET bits

  00 : no offset

  01 : +25mV

  1x : -25mV

Is above correct?

If any missing, please let me know.

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,650件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

shortly, yes in general understanding is right. Also one

needs to set DISABLE_STEPPING and set TRG -

voltage level of the linreg supply.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,651件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

shortly, yes in general understanding is right. Also one

needs to set DISABLE_STEPPING and set TRG -

voltage level of the linreg supply.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信