Question, i.MX233 power supply

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, i.MX233 power supply

Jump to solution
1,698 Views
Aemj
Contributor IV

Hi team,

I would like to ask about power supply feature of i.MX233.

Could you show me the settings for using internal linear regulator outputs of i.MX233 and stopping internal DCDC outputs?

In my customer’s understanding, to stop DCDC output;

- ENABLE_DCDC bit should be cleared.

To use internal linear regulators;

- 5V should be present.

- ENABLE_LINREG bit should be set.

To adjust offset voltage of the linear regulator output;

- set LINREG_OFFSET bits

  00 : no offset

  01 : +25mV

  1x : -25mV

Is above correct?

If any missing, please let me know.

Thanks,

Miyamoto

Labels (1)
0 Kudos
Reply
1 Solution
1,633 Views
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

shortly, yes in general understanding is right. Also one

needs to set DISABLE_STEPPING and set TRG -

voltage level of the linreg supply.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,634 Views
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

shortly, yes in general understanding is right. Also one

needs to set DISABLE_STEPPING and set TRG -

voltage level of the linreg supply.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply