Question about the Boot speed.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about the Boot speed.

Jump to solution
1,251 Views
takashitakahash
Contributor III

Hi community.

Our customer has below question.

This is a question about the boot speed.

QSPI or eMMC selected as a Boot Device, after the POR_B signal De-assert ,how many time from first Access time?

Labels (1)
0 Kudos
Reply
1 Solution
1,145 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

it is about 8-10ms

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,146 Views
igorpadykov
NXP Employee
NXP Employee

Hi Takashi

it is about 8-10ms

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply