Question about qspi-nor-xxx-config file

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Question about qspi-nor-xxx-config file

跳至解决方案
3,826 次查看
ko-hey
Senior Contributor II

Hi all,

 

I need to edit following files because my customer use N25Q032A of micron.

 

qspi-nor-macronix-mx25l51245g-config

qspi-nor-micron-n25q256a-config

qspi-nor-spansion-s25fl128s-config

 

I have a question about parameter of " ddr_mode_enable=1".

 

 

Accessing the NOR flash in DTR / DDR mode when "ddr_mode_enable = 1" is set in the QuadSPI setting file and only ADDR or READ is used without using ADDR_DDR or READ_DDR with lut [n] Is it possible?

 

Ko-hey

 

0 项奖励
回复
1 解答
3,295 次查看
igorpadykov
NXP Employee
NXP Employee

not.

Setting value of ddr_mode_enable requires usage only ddr commands:

ADDR_DDR or READ_DDR.

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
6 回复数
3,295 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

>Accessing the NOR flash in DTR / DDR mode when "ddr_mode_enable = 1"
>is set in the QuadSPI setting file and only ADDR or READ is used without using
>ADDR_DDR or READ_DDR with lut [n] Is it possible?

sorry this is not possible.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
3,295 次查看
ko-hey
Senior Contributor II

Hi igorpadykov

Which mode is used to access the NOR flash when "ddr_mode_enable = 1" is set in the QuadSPI setting file and only ADDR or READ is used with lut [n], SDR mode or DDR mode ?

Ko-hey

0 项奖励
回复
3,295 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

when "ddr_mode_enable = 1" it is necessary to use "ddr" mode commands only:

ADDR_DDR or READ_DDR. ADDR or READ can not be used in "ddr" mode.


Best regards
igor

0 项奖励
回复
3,295 次查看
ko-hey
Senior Contributor II

Hi igorpadykov

When using the ADDR or READ command, it is executed in SDR mode regardless of the setting value of ddr_mode_enable.

Am I correct ?

Ko-hey

0 项奖励
回复
3,296 次查看
igorpadykov
NXP Employee
NXP Employee

not.

Setting value of ddr_mode_enable requires usage only ddr commands:

ADDR_DDR or READ_DDR.

Best regards
igor

0 项奖励
回复
3,295 次查看
ko-hey
Senior Contributor II

Hi igorpadykov

Thank you for your support.

I posted another question (https://community.nxp.com/thread/490304) related to this thread.

I hope you will follow it.

Ko-hey

0 项奖励
回复