Question about profinet solution with IMX processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about profinet solution with IMX processor

2,215 Views
petertao
Contributor I

Hi, Sir: Now I am searching for some solution for profinet, I am wondering if IMX processor could be one of my choice. My questions are:

  1. If IMX could work for profinet solution. If the answer is yes, is there any additional fee(like license) we need to pay if we want to develop the profinet solution with IMX processor.

  2. We may need wifi, How can IMX processor support wifi? I don’t find any details comments in IMX page. 

Could you help me get some comments?

0 Kudos
Reply
2 Replies

2,019 Views
igorpadykov
NXP Employee
NXP Employee

Hi Peter

- i.MX do not support profibus natively. One can consider for

example LS1021 or other QorIQ processor

Single-chip PROFIBUS Reference Platform|NXP

- wifi is supported by using external wifi module connected

to SD or PCIe interfaces

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,019 Views
petertao
Contributor I

Hi, Dear Sir:

Thanks for your response. Could you help me know if there is any solution of IMX processor with 2 ethernet interface?

Best regards!

Tao Xi (Peter)

Siemens Ltd., China

CT DD DS AA CN DI SZ

328 Xinghu Street

215123 SUZHOU, China

Mobil: +86 13814889225

mailto:[email protected]

0 Kudos
Reply