Question about i.MX6SDL EB804.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about i.MX6SDL EB804.

ソリューションへジャンプ
1,864件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

I have a question about i.MX6SDL EB804.

Chapter 3.1 says "To ensure that the new chip revision can be read backfrom the chip, the following patch should be applied.".

http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/commit/?h=imx_3.0.35_4.1.0&id=21464af587...

I checked the above patch, and it adds chip revisions (1.3, 1.4, and 1.5) to BSP.

Then, according to Table 1 of EB804, the i.MX6SDL new silicon revision 1.2 is 0x00000012 in USB_ANALOG_DIGPROG.

In this case, the added chip revisions (1.3, 1.4 and 1.5) are not used when rev 1.2 chip is used.

So I felt the patch is not necessary for rev 1.2 chip.

Is this right?

Best Regards,

Satoshi Shimoda

ラベル(2)
0 件の賞賛
返信
1 解決策
1,748件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes for i.MX6SDL latest revision 1.2,

so patches for other (1.3, 1.5) are not needed.

Please note that Linux BSP is unified for all i.MX6 processors

so this patch is suggested to apply for providing universal solution

for all i.MX6 processors.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,749件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

yes for i.MX6SDL latest revision 1.2,

so patches for other (1.3, 1.5) are not needed.

Please note that Linux BSP is unified for all i.MX6 processors

so this patch is suggested to apply for providing universal solution

for all i.MX6 processors.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信