Question about compatible SD Card.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about compatible SD Card.

ソリューションへジャンプ
2,378件の閲覧回数
inhojeon
Contributor III

Hi, All.

I have a question about compatible SD card for Boot to I.MX6 Dual lite.

I purchased new SD Card is not compatible.

Only compatilbe SD Card is offered to SABRE Bd.

Please, Let me inform compatible SD Card specifications for I.MX6 Dual lite to boot.

Best resards,

Inho Jeon

ラベル(1)
タグ(1)
1 解決策
2,241件の閲覧回数
inhojeon
Contributor III

Hi, Yuri.

Thank you for your replay.

And, Please, Refer to Below this.

That is my question about SD Compatible last 2days.

http://www.samsung.com/sec/consumer/it/storage-2/storage-2/MB-SP16D/KR (MB-SP16D) => Not Compatible  SD Card.

Best Regards,

Inho Jeon

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,241件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

"Boot code supports high capacity and low capacity SD/eSD/SDXC cards ..."

Please refer to section 8.5.3.3 (SD, eSD and SDXC) of the i.MX6 S/DL RM

for more details. Perhaps the problem with new SD cards relates to boot SD
preparation procedure. Please use NXP Linux / Android documentation about it.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,242件の閲覧回数
inhojeon
Contributor III

Hi, Yuri.

Thank you for your replay.

And, Please, Refer to Below this.

That is my question about SD Compatible last 2days.

http://www.samsung.com/sec/consumer/it/storage-2/storage-2/MB-SP16D/KR (MB-SP16D) => Not Compatible  SD Card.

Best Regards,

Inho Jeon

0 件の賞賛
返信
2,240件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

Sometimes full SD card clearing, say using Linux command DD (if=/dev/zero),

before deploying image, helps.

Regards,

Yuri.

0 件の賞賛
返信