Question about compatible SD Card.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about compatible SD Card.

Jump to solution
2,474 Views
inhojeon
Contributor III

Hi, All.

I have a question about compatible SD card for Boot to I.MX6 Dual lite.

I purchased new SD Card is not compatible.

Only compatilbe SD Card is offered to SABRE Bd.

Please, Let me inform compatible SD Card specifications for I.MX6 Dual lite to boot.

Best resards,

Inho Jeon

Labels (1)
Tags (1)
1 Solution
2,337 Views
inhojeon
Contributor III

Hi, Yuri.

Thank you for your replay.

And, Please, Refer to Below this.

That is my question about SD Compatible last 2days.

http://www.samsung.com/sec/consumer/it/storage-2/storage-2/MB-SP16D/KR (MB-SP16D) => Not Compatible  SD Card.

Best Regards,

Inho Jeon

View solution in original post

0 Kudos
Reply
3 Replies
2,337 Views
Yuri
NXP Employee
NXP Employee

Hello,

"Boot code supports high capacity and low capacity SD/eSD/SDXC cards ..."

Please refer to section 8.5.3.3 (SD, eSD and SDXC) of the i.MX6 S/DL RM

for more details. Perhaps the problem with new SD cards relates to boot SD
preparation procedure. Please use NXP Linux / Android documentation about it.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,338 Views
inhojeon
Contributor III

Hi, Yuri.

Thank you for your replay.

And, Please, Refer to Below this.

That is my question about SD Compatible last 2days.

http://www.samsung.com/sec/consumer/it/storage-2/storage-2/MB-SP16D/KR (MB-SP16D) => Not Compatible  SD Card.

Best Regards,

Inho Jeon

0 Kudos
Reply
2,336 Views
Yuri
NXP Employee
NXP Employee

Hello,

Sometimes full SD card clearing, say using Linux command DD (if=/dev/zero),

before deploying image, helps.

Regards,

Yuri.

0 Kudos
Reply