Question about SDB Schematic

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about SDB Schematic

ソリューションへジャンプ
3,044件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I want to know a purpose of using NC7SP125P5X.

NC7SP125P5X have been used for SABRE-SDB.

Please see a MCIMX6Q-SMART DEVICE BOARD schematic in P21.

I think it will be used for reset a PMIC by watchdog-timer.

Please tell me a purpose of using NC7SP125P5X.

Ko-hey

ラベル(2)
タグ(2)
1 解決策
2,838件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

you are right: NC7SP125P5X is used for reset PMIC by watchdog.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,839件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

you are right: NC7SP125P5X is used for reset PMIC by watchdog.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,838件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thank you for your quick response.

As that case, I can't understand the reason why the C504 is needed.

Why C504 is needed ?

ko-hey

0 件の賞賛
返信
2,838件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

it is used for generation of short pulse

Best regards

igor

2,838件の閲覧回数
ko-hey
Senior Contributor II

Hi Igor

Thanks !

ko-hey

0 件の賞賛
返信