Question about SDB Schematic

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about SDB Schematic

Jump to solution
2,189 Views
ko-hey
Senior Contributor II

Hi all

I want to know a purpose of using NC7SP125P5X.

NC7SP125P5X have been used for SABRE-SDB.

Please see a MCIMX6Q-SMART DEVICE BOARD schematic in P21.

I think it will be used for reset a PMIC by watchdog-timer.

Please tell me a purpose of using NC7SP125P5X.

Ko-hey

Labels (2)
Tags (2)
1 Solution
1,983 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

you are right: NC7SP125P5X is used for reset PMIC by watchdog.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
1,984 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

you are right: NC7SP125P5X is used for reset PMIC by watchdog.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,983 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for your quick response.

As that case, I can't understand the reason why the C504 is needed.

Why C504 is needed ?

ko-hey

0 Kudos
Reply
1,983 Views
igorpadykov
NXP Employee
NXP Employee

Hi ko-hey

it is used for generation of short pulse

Best regards

igor

1,983 Views
ko-hey
Senior Contributor II

Hi Igor

Thanks !

ko-hey

0 Kudos
Reply