Question about RPMsg

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about RPMsg

4,057件の閲覧回数
xu_ji1
Contributor V

Hello,

I want to ask that A core communicate with M4 core use RPMsg SW side,and for HW side is it used MU in M4 or MU

in A core LSIO or both used in M4 and A core?

Thanks

ラベル(2)
タグ(1)
0 件の賞賛
返信
7 返答(返信)

3,665件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

In which i.MX chip are you working?

Best regards,

Diego.

0 件の賞賛
返信

3,665件の閲覧回数
xu_ji1
Contributor V

Hello,

The chip is I.MX8QXP which I used.

Thanks

0 件の賞賛
返信

3,665件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

Unfortunately, the i.MX8QX is still on preproduction and we do not have any official information available for the moment. I apologize for the inconveniences this could give you.

 Best regards,

Diego.

0 件の賞賛
返信

3,665件の閲覧回数
xu_ji1
Contributor V

Hello,

How about i.MX7 chip?

Thanks

0 件の賞賛
返信

3,665件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

For the i.MX7. The RPMsg is the Linux API that is in charge of communicating the core A7 and M4. The RPMsg is a virtio-based messaging bus, which allows kernel drivers to communicate with remote processors available on the system. 

The MU is the unit module from the i.MX that enables two processors within the SoC to communicate and
coordinate by passing messages (e.g. data, status and control) through the MU interface.

Hope this information could help you.

Best regards,

Diego.

0 件の賞賛
返信

3,665件の閲覧回数
xu_ji1
Contributor V

Hello,

Then the MU unit is a sub module in core A7 or M4 in i.MX7 ?

Thanks

0 件の賞賛
返信

3,665件の閲覧回数
diegoadrian
NXP Employee
NXP Employee

Hello,

On the i.MX7D, the A7 is the core principal of the i.MX. Every other peripheral, including the cortex M4, are submodules. However, the MU is the module that is in charge of coordinate by messages both cortex.

Hope this can help you.

Best regards,

Diego.

0 件の賞賛
返信