Question about Length Calculation of Clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about Length Calculation of Clock

1,097 Views
thomasstockklau
Contributor I

Hello MX users,

i have a question about the i.MX6 Routing, actually i have matched all Lines but i need a Informations about the Clock Length Calulation.

Whath of the following 2 calculation sheems is the Right:

1. With Termination Resistor Length

i get A Complete Length of 2120 mils per Clock Line ( CLK X + /-)

2. Without Termination Resistor Length

i get a Complete Length of 2450 mils per Clock Line ( CLK X + /-)

What is the right value? I need it for the Rule Adress = max Clock -200 mils...

Thank you for Helping

ddr3.jpg

Labels (6)
Tags (3)
0 Kudos
Reply
1 Reply

959 Views
igorpadykov
NXP Employee
NXP Employee

Hi Thomas

right calculation is without Termination Resistor Length R.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply