Question about IMX6Q display interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about IMX6Q display interface

Jump to solution
4,011 Views
alex_li
Contributor II

Some question about display interface of IMX6Q:

1: As meationed in data sheet "Up to four interfaces may be active in parallel"  and external signal describes in Reference Manual "Table 37-6. IPU1 External Signals" , can i connect 2 display panel via 24bpp RGB LCD Display interface(IPU1-DI0 & DIi1)

1.bmp

2: As external signal describes in Reference Manual "Table 37-7. IPU2 External Signals", IPU2 only support DI0 and data port is use same pad with IPU1-DI0,is it right?

2.png

3:Want connect 4 display panel via 2X 24bpp RGB LCD Display interface & 2X LVDS,is it possible?

Thanks very much!

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
3,718 Views
igorpadykov
NXP Employee
NXP Employee

Hi min

in general i.MX6Q has 2 IPU modules and 2 display panel via 24bpp RGB LCD can

be supported, provided there are external signals for these interfaces, please check

Table 4-1. Pin Assignments i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

May be useful to use PINS-TOOL :

Pins Tool for i.MX Application Processors|NXP 

2 lvds also supported according to Table 39-3. LDB External Signals.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
6 Replies
3,719 Views
igorpadykov
NXP Employee
NXP Employee

Hi min

in general i.MX6Q has 2 IPU modules and 2 display panel via 24bpp RGB LCD can

be supported, provided there are external signals for these interfaces, please check

Table 4-1. Pin Assignments i.MX6DQ Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMX6DQRM.pdf

May be useful to use PINS-TOOL :

Pins Tool for i.MX Application Processors|NXP 

2 lvds also supported according to Table 39-3. LDB External Signals.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
3,718 Views
alex_li
Contributor II

Thanks igor!

Answer of Q1&2 is very clear.

Q3" IMX6Q can support 4 display panel via 2*24bpp RGB LCD + 2*LVDS at the same time.Is it right?" need be confirm again.

Best regards

min li

0 Kudos
Reply
3,717 Views
igorpadykov
NXP Employee
NXP Employee

Hi min

please use PINS-TOOL  to check if such mux option is possible.

Best regards
igor

0 Kudos
Reply
3,717 Views
alex_li
Contributor II

igor:

   no error report when use Pins Tool.Thanks again!!!

min li

0 Kudos
Reply
3,718 Views
igorpadykov
NXP Employee
NXP Employee

Hi min

 

if PINS-TOOL does not report mux option problems, then this is possible.

 

Best regards
igor

0 Kudos
Reply
3,718 Views
alex_li
Contributor II

Thanks igor!

0 Kudos
Reply