Question about DCD setting in imximage.cfg

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question about DCD setting in imximage.cfg

1,569件の閲覧回数
ko-hey
Senior Contributor II

Hi all

I want to clarify DDR initialization for i.MX7D so I'm checking the following file.

uboot-imx.git - Freescale i.MX u-boot Tree 
There are two registers which is not described in reference manual as below.

/* Clear then set bit30 to ensure exit from DDR retention */
DATA 4 0x30360388 0x40000000
DATA 4 0x30360384 0x40000000


Q1
What function of those registers ?
According to the section 2.1.5 AIPS Memory Map, it supposed to be CCM Analog register.
However, there are no description in RM so please tell me the function of the register.

Q2
Why do you set 0x40000000 to 0x30360388 and 0x30360384 ?


Q3
I also checked following thread.
Do I need to post this question to SR ?
https://community.nxp.com/message/870552

Ko-hey

ラベル(3)
0 件の賞賛
返信
1 返信

1,308件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

  I sent You some information directly via e-mail.

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信