Question, SPI flash memory addressing mode for i.MX28

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question, SPI flash memory addressing mode for i.MX28

ソリューションへジャンプ
1,856件の閲覧回数
Aemj
Contributor IV

Dear team,

I would like to ask about the addressing of SPI flash memory used for i.MX28 boot device.

My customer plans to use SPI flash memory for boot storage of their i.MX28 board.

Is it possible to use 256Mbits SPI flash for that?

That is,

Is it possible to use SPI flash with its 4byte addressing mode?

Thanks,

Miyamoto

ラベル(1)
0 件の賞賛
返信
1 解決策
1,251件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

i.MX28 supports only 3byte addressing as

described in sect.12.10 SPI Boot Mode MCIMX28RM

supports only 2-byte addresses for EEPROMs and 3-byte addresses for NORs.

I think you can consult with this flash vendor support if it supports also 3byte addressing mode.

Best regards

igor

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,252件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi AVNET JAPAN FAE

i.MX28 supports only 3byte addressing as

described in sect.12.10 SPI Boot Mode MCIMX28RM

supports only 2-byte addresses for EEPROMs and 3-byte addresses for NORs.

I think you can consult with this flash vendor support if it supports also 3byte addressing mode.

Best regards

igor

0 件の賞賛
返信