Question: HTML5(really CSS3) on imx6 SD?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Question: HTML5(really CSS3) on imx6 SD?

3,225件の閲覧回数
Jetcitycowboy
NXP Employee
NXP Employee

   I have a customer currently in the process of porting Android to our i.MX6 platform and have noticed that the WebKit HTML5 performance is very poor.  Similar performance  is demonstrated on the SabreSD as well as custom HW, on both ICS and JB.

   (Technically it is CSS3 transitions, not HTML5. The term HTML5 tends to encompass CSS3. )

If you go to a few simple HTML5 demos such as:

http://www.apple.com/html5/showcase/transitions/

http://www.juicebox.net/demos/pro/slider/

On i.MX6 the transitions are very jerky, and sometimes don't even happen. Is Android using the GPU for these transitions?  It is evident that the opengl libraries are being loaded when a browser is opened  but it is not clear  if the HTML5 transitions specifically are using the GPU.

Examples have been tested on various phones and tablets running Android and smooth transitions are indicated. It is expected the performance of the i.MX6 to be comparable to the Android devices on the market today.

Please let me know if anyone hase any  specific insigh as to the mechanism and optimization involved in these processes.

ラベル(2)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,591件の閲覧回数
FranciscoCarril
Contributor V

What browser within Android are you using to test?  It seems this is browser dependent.

Here some examples:

html5 - What exact parts of CSS3 are GPU accelerated? - Stack Overflow

2,591件の閲覧回数
Jetcitycowboy
NXP Employee
NXP Employee

The default Android browser, which uses the built-in WebView, which is based on WebKit within the Android sources.

Good suggestion, using the Chrome app seems to be a lot better. Still a bit jerky though .We are looking into it more.

0 件の賞賛
返信