Query on the Tamper Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Query on the Tamper Pin

1,969 Views
puneethkumar
Contributor III

Dear Team,

There are total 10 tamper pins together in the application processor which i am using.

I am planning to use only two pins a tamper, other pins as the GPIO's.

It is mentioned like this in the datasheet for the power section of tamper pins.

" VDD_TMPR_CSI_1P8_3P3 Shall be connected to VDD_SNVS_LDO_1P8_CAP when used as a
tamper pin. In CSI mode use an external 1.8 V supply. In this case, follow the 1.8 VI/O specification above."

If i want to use the above case ( i.e two as a tamper pin & other as GPIO) what should be the power domain to VDD_TMPR_CSI_1P8_3P3.

Thanks in advance.

0 Kudos
Reply
3 Replies

1,947 Views
puneethkumar
Contributor III

Thanks for the reply

If i make above connection will i able to use tamper pins both as GPIO & tamper detection pins

1,944 Views
Yuri
NXP Employee
NXP Employee

@puneethkumar 
Hello,

  It is recommended to use VDD_SNVS_LDO_1P8_CAP as voltage source
for the tamper pins in order to be able to detect tampers in low power modes.
 If there are not requirements to detect events in low power modes, any
voltage source may be applied.

Regards,
Yuri.

0 Kudos
Reply

1,959 Views
Yuri
NXP Employee
NXP Employee

@puneethkumar 
Hello,

  connect  VDD_TMPR_CSI_1P8_3P3 to VDD_SNVS_LDO_1P8_CAP.

Regards,
Yuri.

0 Kudos
Reply