Query on PF3001 and PF3000 related circuit

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Query on PF3001 and PF3000 related circuit

1,479 次查看
vineethhegde
Contributor II

Hi,

I have below queries on PF3001 and PF3000 circuit

1. The PF3001 and PF3000 are footprint compatible. But the some pin assignments are different.

    In PF3001 the 24,25th pins are GND and NC

    In PF3000 the 24,25th pins are VREFDDR and  VINREFDDR.

So how VREFDDR is generated in the PF3001 if we are not using resistor divider circuit. 

2.  As observed in datasheet of PF3001 24th pin is GND and in PF3000 VINREFDDR so as observed in schematics when we are mounting PF3001 24 pin will be supplied by voltage rail  DRAM_1V35(SW3 output). Please clarify.

Regards,

Vineeth 

标签 (2)
0 项奖励
回复
3 回复数

1,293 次查看
vineethhegde
Contributor II

Hi,

As per the recomondation mentioned in the PF3001 datasheet Pin 24 is GND and recommended to connected to Ground. But for PF3000 24th Pin is VINREFDDR. How this is taking care in the schematics compatible for both the chips. The schematics i reffered is SPF-29090_C.

Regards,

Vineeth

0 项奖励
回复

1,293 次查看
Yuri
NXP Employee
NXP Employee

Hello,

  

  I would prefer to use the recent Datasheet recommendations.

Regards,

Yuri.

0 项奖励
回复

1,293 次查看
Yuri
NXP Employee
NXP Employee

Hello

  PF3001 is pin compatible with PF3000 - this allows to use the same board ( say, with

configuration jumpers) for both ones. But PF3001 does not provide specially DDR reference

voltage. External circuit is needed for it.

  Please follow PF3001 DataSheet recommendations regarding pin connections / termination,

when using the PF3001.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 项奖励
回复