Qt5 library

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Qt5 library

2,020 次查看
adelantesey
Contributor IV

Dear friends,

i wanted to run qt app on ms6sabresd. i wrote a helloworld (console app) im my PC and cross-compiled it for imx6sx

when i attempt to run the app om the target. it says "libQt5core.so.5 not found"  also i guess it will be the same if i use widget. the embedded target is connect to my PC through NFS and the rootfs is on PC.

do i need new rootfs? or should i some how install library for qt on it?

do i need to use yocto to build rootfs? if yes which image should i use? (i work with fsl-community-bsp)

thank you all in advanced

标签 (3)
0 项奖励
回复
3 回复数

1,540 次查看
joanxie
NXP TechSupport
NXP TechSupport

what image do you build? let me reminder, you should build fsl-image-qt5 which includes qt5.

0 项奖励
回复

1,540 次查看
adelantesey
Contributor IV

thanks, but this image is not in fsl-community-bsp (it says : nothing provides fsl-image-qt5)

is there a way to skip bitbaking everything from the start? i mean is it possible to install the qt lib on the existing rootfs?

thanks again.

0 项奖励
回复

1,540 次查看
joanxie
NXP TechSupport
NXP TechSupport

you can build the qt on imx6q, pls refer to the document as below:

https://community.nxp.com/docs/DOC-94066 

0 项奖励
回复