Hello,
Currently I am working on imx6-yocto qt5 porting on phytec's phyflex imx6 target. Here I have changed 3.19 kernel to 3.14 kernel for some customization purpose, but qt5 demos are not working when i load 3.14 kernel. I am not using inside yocto project kernel except rootfs.Please can give any information in this case.
*******************************************************************************************************
root@phyboard-subra-imx6-1:~# qt5demo-starter
QEglFSImx6Hooks will set environment variable FB_MULTI_BUFFER=2 to enable double buffering and vsync.
If this is not desired, you can override this via: export QT_EGLFS_IMX6_NO_FB_MULTI_BUFFER=1
[ 1] HAL user version 5.0.11 build 19959 Aug 6 2014 03:02:58
[ 2] HAL kernel version 5.0.11 build 25762
Segmentation fault
root@phyboard-subra-imx6-1:~#
********************************************************************************************************
Thanks & Regards,
Narasimha
Hello,
Currently I am facing this the below issue. Please anuggest any inputs.
root@imx6qsabresd:~#
root@imx6qsabresd:~#
ocks@imx6qsabresd:~# /usr/share/qt5/examples/widgets/animation/moveblocks/moveblo
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.
Unable to find an X11 visual which matches EGL config 1
Thanks & Regards,
Narasimha
Hi jimmychan,
Thanks for your reply. Here actually for the kernel BSP customization purpose only builded outside. Can you guide me how to switch the kernel in yocto
BSP to "imx_3.14.28_1.0.0_ga" branch which will supports dual display also.
Thanks & Regards,
Narasimha
Attached is the Yocto User guide. In section 5.6, there is a 'repo init' command to download the kernel source code. The -b <branch name> option used for downloading the kernel from different branch. For your information, here is the list of Branch of different i.MX kernel version. linux-2.6-imx.git - Freescale i.MX Linux Tree