Qt5 Video Playback using XCB Backend

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Qt5 Video Playback using XCB Backend

2,402 Views
JustinWaters
Contributor III

Has anybody successfully played video in the QtMultimediaWidgets player application while using the xcb backend? I've found a number of posts regarding video playback in Qt5 with the VPU acceleration, but most of them seem to require disabling X11.

When I try using XCB, the video simply hangs while loading the video:

root@imx6qsabresd:~# /usr/share/qt5/examples/multimediawidgets/player/player /BigBuckBunny.avi

Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.

Qt Warning: Could not find a location of the system's Compose files. Consider setting the QTCOMPOSE environment variable.

Aiur: 3.0.11

Core: AVI_PARSER_03.05.12  build on Jul 15 2014 02:45:03

  mime: video/x-msvideo

  file: /usr/lib/imx-mm/parser/lib_avi_parser_arm11_elinux.so.3.1

Content Info:

        URI:

              file:///BigBuckBunny.avi

        Idx File:

              /home/root/.aiur/.BigBuckBunny.avi.aidx

        Seekable  : Yes

        Size(byte): 1370826

Movie Info:

        Seekable  : Yes

        Live      : No

        Duration  : 0:00:32.496326000

        ReadMode  : Track

        Track     : 2

Track 00 [video_000000] Enabled

        Duration: 0:00:32.480000000

        Language: und

        Mime:

              video/mpeg, mpegversion=(int)4, parsed=(boolean)true, width=(int)320, height=(in

              t)240, framerate=(fraction)25/1

[INFO]  Product Info: i.MX6Q/D/S

vpudec versions :smileyhappy:

        plugin: 3.0.11

        wrapper: 1.0.46(VPUWRAPPER_ARM_LINUX Build on Feb 12 2015 15:09:45)

        vpulib: 5.4.23

        firmware: 3.1.1.46056

Track 01 [audio_000000] Enabled

        Duration: 0:00:32.496326000

        Language: und

        Mime:

              audio/mpeg, mpegversion=(int)1, framed=(boolean)true, channels=(int)1, rate=(int

              )22050, bitrate=(int)0

Beep: 3.0.11

Core: MP3 decoder Wrapper  build on Mar 21 2014 15:04:50

  mime: audio/mpeg, mpegversion = (int)1

  file: /usr/lib/imx-mm/audio-codec/wrap/lib_mp3d_wrap_arm12_elinux.so.3

CODEC: BLN_MAD-MMCODECS_MP3D_ARM_02.13.00_CORTEX-A8  build on Apr 10 2014 15:26:15.

If I set GST_DEBUG=2, I get the following warning over and over again:

aiurdemux /home/justin/work/yocto/build/tmp/work/imx6qsabresd-poky-linux-gnueabi/gst-fsl-plugin/3.0.11-r0/gst-fsl-plugins-3.0.11/src/parser/aiur/src/aiurdemux.c:4095:aiurdemux_push_pad_buffer: Pad video push error type -4

The same video plays fine using gplay, playbin2, and a standard manual gstreamer pipeline. I'm using the head of line for all of the metalayers (include meta-qt5). I synced the repo yesterday. I did have to disable the gstreamer1.0 patches (I'm using gstreamer 0.10) in the qtmultimedia recipe.

Tags (3)
4 Replies

1,724 Views
JustinWaters
Contributor III

If it helps, here's more information about what I'm currently using:

meta-fsl-arm-extra dizzy

meta-fsl-arm dizzy

meta-qt5 master (commit adeaa6128b665920eb98eb7c064f4aacbd74b873)

Qt5.4

Linux 3.10.17

gstreamer 0.10.36

gst-fsl-plugins 3.0.11

libfslcodec 4.0.1

0 Kudos
Reply

1,725 Views
OtavioSalvador
Senior Contributor II

We are in some projects, for customers, using QtMultimedia. In our case we used the QML based plugin and it works fine.

Check the qmlvideofx or similar and see if it works for you.

1,725 Views
JustinWaters
Contributor III

Thank you very much for the reply.

The qmlvideofx player does seem to work. Any clue as to why the non-QML version hangs? I think we can work with the QML-based version moving forward, but understanding the limitations/shortcomings of the other player will be helpful in future projects.

0 Kudos
Reply

1,725 Views
OtavioSalvador
Senior Contributor II

I didn't investigate as our customer is using QML.

0 Kudos
Reply