Hi all:
I’m now trying to build a media player on a ARM board, the cpu is freescale iMX6. System on board is ubuntu 12.04. And I have build a cross compiler for the board on my PC which is also running 12.04.
 I’ve built a small program using QSound to play a wav file successfully on my computer.
 But when I tried to compile it with cross compiler, a notice reads: “ Project ERROR: Unknown module(s) in QT: multimedia “ appeared. 
 In my .pro file, I’ve added QT += widgets multimedia.
 And I’ve include <QSound> in my main.cpp.
 And I’ve checked the cross compiler libs, there’s QSound there. 
When compile programs for PC, I use g++.
 And for the arm system, I use arm-fsl-linux-gnueabi-gcc.
I build the Qt5 cross compiler according to the website:
https://community.freescale.com/docs/DOC-94066
So does anyone meet the same problem?
 Do I need to set more parameters?
 Thanks a lot.
And I've check the ../qt5/qtbase/mkspecs/modules
There's no file like qt_lib_multimedia.pri.
Is this the cause of the problem?
How can I install it back?
Thanks.