Qt application Development on iMX8

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Qt application Development on iMX8

6,169件の閲覧回数
kvk0422
Contributor II

Hi, 

We are using QT creator 4.8.2 for QT application for our target device NXP i.MX8MQ.
NXP i.MX8MQ is having linux 4.9.88_2.0, when we are trying to add target to QT device Kit, we are not able to flash simple QT code to target (NXP i.MX8MQ).
Can you please guide us how to flash Qt code to i.MX8MQ. Sampled code is attached, please verify and modify for any changes.

Should we build Qt from scratch? Any sample qt framework which can readily flash to i.MX8MQ board running with Linux.

Can you please confirm Boot2QT 5. 11.2 NXP i.MX8QM which is available in Qt Maintence tool is fully functional? is their any missing files in the Image?

.

Thanks in advance for your help.

Varun K

0 件の賞賛
返信
3 返答(返信)

5,431件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello varun,

The MX8 use QT 5.10 in xwayland, you just need compile your project inside the qt environment, remember meta-imx-liri is not fully tested but also it can helps

Regards

0 件の賞賛
返信

5,430件の閲覧回数
kvk0422
Contributor II

Hi Alfred, 

Thank you for your reply. Can you please provide any document or steps to follow to xwayland for imx8. 

Thanks in advance for your help.

Regards,

Varun 

0 件の賞賛
返信

5,430件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi,

The yocto project user guide might help you, is installed on you documentation folder.

Regards

0 件の賞賛
返信