Hi, NXP and everyone
For IMX6ULL, I'm using fsl-imx-wayland(4.1.15-2.0.1).
I tested Qt example "Cube", in mainwidget.cpp, MainWidget::paintGL() function running of consume 350ms, and MainWidget::timerEvent() interval was set with 12ms but actually is 4500ms (when MainWidget::paintGL() is empty, it is 11~14ms). So, the scene is drawn with 4.5s interval, too slow.
Please help me to solve this problem.
Best Regards,
Thanks, aither