QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled

7,893 Views
andreykononov
Contributor III

i'm trying to start app on i.mx6 with yocto X11 build image but get error

root@imx6qsabreauto:~# Qt5_CinematicExperience

libpng warning: iCCP: known incorrect sRGB profile

libpng warning: iCCP: known incorrect sRGB profile

QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled

Failed to create OpenGL context for format QSurfaceFormat(version 2.0, options QFlags(), depthBufferSize 24, redBufferSize -1, greenBufferSize -1, blueBufferSize -1, alphaBufferSize -1, stencilBufferS

/usr/bin/Qt5_CinematicExperience: line 4:   517 Aborted                 /usr/share/cinematicexperience-1.0/Qt5_CinematicExperience $*

googling nothing useful given

0 Kudos
Reply
1 Reply

4,629 Views
igorpadykov
NXP Employee
NXP Employee

Hi Andrey

nxp provides proprietary package "fslqtapplications", refer to attached Release Notes, BSP on link

Board Support Packages (29)

L3.14.52_1.1.0_MX6QDLSOLO (REV L3.14.52_1.1.0)

http://www.nxp.com/products/microcontrollers-and-processors/arm-processors/i.mx-applications-process...

steps to build X11

https://community.freescale.com/docs/DOC-330047

I am afraid that anything above will require special support with third parties or NXP Professional Services:

http://www.nxp.com/support/nxp-professional-services:PROFESSIONAL-SERVICE

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply