QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled

7,491 Views
alonghong
Contributor I

Hi Sir

I use the iMX8QM EVK and follow imx-yocto-L4.14.98_2.0.0_ga user'guide.

I can success to use SV3D-1.1 sample.

Now,I want to use QT to design the UI, so I use fsl-image-qt5-validation-imx to support QT5.

and I can use cross compile to test the qt project on iMX8 EVK.

 But, when I use the OpenGL like QOpenGLWidget or QGLWidget on QT project, the terminal will show

as below:

"QXcbIntegration: Cannot create platform OpenGL context, neither GLX nor EGL are enabled'

I check the fsl-image-qt5-validation-imx image QT5 example, the path is /usr/share/qt5/examples/opengl/hellogl2/./hellogl2.

It has the same problem.

Please kindly to help me to solved this question

thanks a lot

Best Regards.

 

0 Kudos
Reply
2 Replies

7,478 Views
alonghong
Contributor I

Hi Bio_TICFSL

I solved this issue, the solution is when I execute my test application, I need to key ./test -platform wayland-egl.

and then the application is work.

but I find another question is when I move the yuv data to  y , u , v array and use the opengl to paint image.

the action spend a lot of time to complete. I don't know what's happened.

please kindly to help me solve this question

thanks a lot

Best Regards.

0 Kudos
Reply

7,484 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello alonghong,

You need to use the L5.4.70 at least to use OpenGL with QT.

Regards

0 Kudos
Reply