QUECTEL EC25E LTE module testing on imx6.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QUECTEL EC25E LTE module testing on imx6.

1,205 次查看
selvamurugantha
Contributor I

I am testing quectel EC25E LTE module on my imx6 board.quectel LTE module will detect as USB.For this,I need to edit option.c file in kernel.I want to add some hex value of EC25E module and add it in kernel.Then it will detect as usb and i will go ahead on another step.Now problem is there is no file like option.c in my kernel .I have few question about this imx6 kernel.I am using linux 3.0.55 kernel on my board.

1)May I download same kernel version and modify the option.c file and add it in kernel.

2)If i will add kernel file like this,in future it will affect reset of the functions of the imx6 or not

So,how to edit option.c and add it in kernel

标记 (3)
0 项奖励
回复
0 回复数