QT5 replacement with other open source packages

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QT5 replacement with other open source packages

1,129 Views
mjaafar
Contributor II

QT provides the graphic interface using wayland / eglfs to create for example menus. It provides also the communication with the camera and several other modules. The Qt can be replaced with gtk.But, the performance related to GTK using SDL is far away lower than QT.

So what is a better replacement with better performance for QT.

Thanks,

0 Kudos
Reply
1 Reply

1,100 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

Qt is the official in this case, if you change you don't have support for it in the official BSP I mean the GPU stuff is attached to qt so It's the best.

Regards

 

0 Kudos
Reply