QT5 Corrupted display output with LTIB 4.1.0 BSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QT5 Corrupted display output with LTIB 4.1.0 BSP

ソリューションへジャンプ
2,443件の閲覧回数
ottob
Contributor IV

Hi There,

I built QT5 according to the instructions posted here -  https://community.freescale.com/docs/DOC-94066. Now I'm attempting to run the sample applications, but the output is corrupted. I attached the a screen cap of what the "knobs" demo looks like. Other ones appears to suffer from the same problem. I tried it on MIPI displays and full 1080P HD LVDS screens, which both work great with gstreamer. I am using imx6q on plain Linux (no X11)


Any ideas on what it could be ?


Thanks,


/Otto

ラベル(4)
タグ(4)
0 件の賞賛
返信
1 解決策
2,104件の閲覧回数
ottob
Contributor IV

For anyone else running into this problem - this solves it. For some reason QT is not smart enough to set up the framebuffer

fbset -g 1920 1080 1920 3240 32

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,104件の閲覧回数
ottob
Contributor IV

Update - If I play a video using gstreamer before starting the QT demo the display looks a lot better. All elements of the demo is located in the correct place, but the colors are way off. This leads me to believe it has something do do with the color format / frame buffer setup. However I'm not sure how to set that up properly.

Any ideas ?

Thanks,

/Otto

0 件の賞賛
返信
2,105件の閲覧回数
ottob
Contributor IV

For anyone else running into this problem - this solves it. For some reason QT is not smart enough to set up the framebuffer

fbset -g 1920 1080 1920 3240 32

0 件の賞賛
返信
2,104件の閲覧回数
ottob
Contributor IV

Also, if you seeing small square boxes instead of text - Install the "Liberation Font" package (LTIB)

0 件の賞賛
返信