QT4.8.6 eglfs Segmentation fault

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QT4.8.6 eglfs Segmentation fault

ソリューションへジャンプ
3,077件の閲覧回数
Wizard_Richard
Contributor II

Hi,

I am porting QT to my mx6q custom board, there are some problems with the eglfs.

 

I use the LTIB package L3.0.35_4.1.0_130816_source.tar.gz and QT4.8 with tag v4.8.6(qtproject/qt · GitHub ).

According to Building QT for i.MX6

To build LTIB, the ipu,vpu and gpu firmware and libraries has been selected.

To build qt4.8.6, the step is:

① ./configure \

  -opensource -confirm-license -release -shared -qpa -arch arm -verbose \

  -xplatform qws/linux-imx6-g++ -fast -optimized-qmake -pch -opengl es2 -egl \

  -qt-sql-sqlite -qt-libjpeg -qt-zlib -qt-libpng -qt-freetype \

  -no-webkit -no-qt3support -exceptions -no-rpath \

  -make examples -make demos -make libs -nomake docs

② make && make install

③ build eglfs and linuxfb libraries.

Then copy all the QT files to LTIB rootfs, then boot through NFS. After that, set some QT environment variables, then run the QT examples.

Firstly, I run some examples with linuxfb, such as "collidingmice -platform linuxfb", it's ok.

But when I run some opengl examples, such as "hellogl_es2 -platform eglfs", I get error message as following:

"Opened display 0x36d844f8

Initialized display 1 4

Segmentation fault"

The same error I use the QT5.4.2, all the opengl examples always can't be executed.

Does any one can help me?

Best Regards,

Richard

ラベル(4)
0 件の賞賛
返信
1 解決策
1,856件の閲覧回数
Wizard_Richard
Contributor II

I have found the problem, The kernel code and the libraries is not matched.

So, I port my custom board from original package L3.0.35_4.1.0_130816_source.tar.gz, then,

run the opengl demo such as "./hellogl_es2 -platform eglfs", it success, about 100fps.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
1,857件の閲覧回数
Wizard_Richard
Contributor II

I have found the problem, The kernel code and the libraries is not matched.

So, I port my custom board from original package L3.0.35_4.1.0_130816_source.tar.gz, then,

run the opengl demo such as "./hellogl_es2 -platform eglfs", it success, about 100fps.

0 件の賞賛
返信
1,856件の閲覧回数
sanjeevsharma
Contributor IV

Hello,

I have similar issue QT5.4 eglfs(hellogl_es2) Segmentation fault

How did you identified that kernel code and EGL libraries is not matched ?

Regards

Sanjeev Sharma

0 件の賞賛
返信
1,856件の閲覧回数
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hi Richard,

Did you successfully add the EGL support patch image? as the Building QT for i.MX6 mention.

0 件の賞賛
返信