QT on yocto build

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QT on yocto build

1,657件の閲覧回数
sachusanal
Contributor III

Hai SIr,

I have mx6qsabresd board with me.I need to run my Qt application on my board. i bitbake core-image-sato-sdk image  for sabresd board . I have yocto daisy image with me how can i configure the QTcreater for compiler and debugeer operation.

please help me  to solve this issue

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,329件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

   Please refer to the following :

Setting up Qt Creator to build for i.MX6


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,329件の閲覧回数
sachusanal
Contributor III

Dear Yuri ,

We have followed the steps  as per the above mentioned documents

Could not start Process

Error while building /Deploying projects when executing step make

Note:

In build &Run -> Qt versions : /opt/poky/1.6.2/sysroots/x86_64-pokysdk-linux/usr/bin/qt5/qmake

at the time we get a notification like no compiler can produce code for this qt version.

could you please help me, to solve this issue

0 件の賞賛
返信

1,329件の閲覧回数
Yuri
NXP Employee
NXP Employee

You may just post this question as comment directly in Setting up Qt Creator to build for i.MX6

Regards,

Yuri.

0 件の賞賛
返信