QT Creator 2.3.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QT Creator 2.3.0

2,239件の閲覧回数
rmeyer_arrow
Contributor II

Hello I'm new to the i.MX area and to using QT.

I have been following the document here: http://imxcommunity.org/forum/topics/qt-4-7-4-embedded-spec-on-i-mx...

The demos are not running but I have that in a different discussion.

Right now I have built the Hello program and it ran on the host machine, Ubuntu 10.4LST.

I made the changes called for in the PDF from the link but when I try to compile now I get some build issues.

  • main.o: Relocations in generic ELF (EM:3)
  • main.o: Relocations in generic ELF (EM:3)
  • could not read symbols: file in wrong format      main.o
  • collect2: ld returned 1 exit status

I have checked all the settings and they seem to be as described in the document but still get the errors.

Did I miss a step?

タグ(2)
0 件の賞賛
返信
2 返答(返信)

2,086件の閲覧回数
rmeyer_arrow
Contributor II

Thank you, I checked the path and it looked correct but I recently rebooted and now it seems to be working.

Not sure what was stuck.

0 件の賞賛
返信

2,086件の閲覧回数
KrishnaPavan
Contributor II

I got past through such errors, by using suitable compilers.

What about you?

0 件の賞賛
返信