QT Creator 2.3.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QT Creator 2.3.0

2,263 次查看
rmeyer_arrow
Contributor II

Hello I'm new to the i.MX area and to using QT.

I have been following the document here: http://imxcommunity.org/forum/topics/qt-4-7-4-embedded-spec-on-i-mx...

The demos are not running but I have that in a different discussion.

Right now I have built the Hello program and it ran on the host machine, Ubuntu 10.4LST.

I made the changes called for in the PDF from the link but when I try to compile now I get some build issues.

  • main.o: Relocations in generic ELF (EM:3)
  • main.o: Relocations in generic ELF (EM:3)
  • could not read symbols: file in wrong format      main.o
  • collect2: ld returned 1 exit status

I have checked all the settings and they seem to be as described in the document but still get the errors.

Did I miss a step?

标记 (2)
0 项奖励
回复
2 回复数

2,110 次查看
rmeyer_arrow
Contributor II

Thank you, I checked the path and it looked correct but I recently rebooted and now it seems to be working.

Not sure what was stuck.

0 项奖励
回复

2,110 次查看
KrishnaPavan
Contributor II

I got past through such errors, by using suitable compilers.

What about you?

0 项奖励
回复