QSPI flash verify error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QSPI flash verify error

1,447件の閲覧回数
yuichi_takeda
Contributor I
Hello, community.
I am trying to implement a writing function to QSPI flash on iMX7Dual.
However, a verify error occurs.
In other words, what is written is different from what is read immediately after.

When I check the memory dump of the debugger, it seems that it is written correctly to the specified address of QSPI flash.
CPU MMU and cache are disabled.

I'm guessing that QSPI flash has memory like cache. And I'm guessing that the flash is written correctly, but the same contents are not reflected in the memory (or vice versa).
If so, please tell me the function, command, etc. that flushes the memory.
What else could be the cause?
Best regards,
Yuichi Takeda
ラベル(2)
0 件の賞賛
返信
0 返答(返信)