Hi Experts,
I am gonna boot my i.mx8m mini evk board using qspi flash not to use tcm. what are the changes i need to do in soc.mak particularly to get flash.bin which it should contain entry address of qspi memory. Is there any manual for get to know imx-mkimage tool? Can you ping that manual, if it is available.
And one more question is How to flash binary into board. shall i use openocd or uuu tool? which one is better
Thank You.
解決済! 解決策の投稿を見る。
Hi,
There is no such document. You can download imx-mkimage
then you can find details that you need from /scripts/qspi_header and mkimage_imx8.c
make the target for, e.g., flash_evk_flexspi that you can find from soc.mak for reference.
and you can refer to RM, such as, Quad SPI Interface.
There is one Flexible Serial Peripheral Interface (FlexSPI) block that acts as an interface
to one or two external Quad SPI serial flash devices, each with up to four bidirectional
data lines.
Regards
Harvey
Hi,
There is no such document. You can download imx-mkimage
then you can find details that you need from /scripts/qspi_header and mkimage_imx8.c
make the target for, e.g., flash_evk_flexspi that you can find from soc.mak for reference.
and you can refer to RM, such as, Quad SPI Interface.
There is one Flexible Serial Peripheral Interface (FlexSPI) block that acts as an interface
to one or two external Quad SPI serial flash devices, each with up to four bidirectional
data lines.
Regards
Harvey
If i initialize flexspi driver, can i able to access qspi(256MB) memory?