QSB not working with U-boot instructions. -blog archive

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QSB not working with U-boot instructions. -blog archive

1,008 Views
captmark
Contributor I

If  follow the instructions from Quick Start Guide for i.MX54 QSB. It appears  that maybe the sync freq is not working. There is a column about 1/5 of the lcd width that has the lcd screen layered in it. I did test the lcd when I first received the kit and the lcd work fine out of the box. I am running same sd card that came with kit. Only change has been toset bootregs to setup lcd.

 

Any ideas.

 

Mar

Tags (1)
0 Kudos
Reply
1 Reply

960 Views
VladanJovanovic
NXP Employee
NXP Employee

Can you share full output of the boot process (u-boot and Linux kernel)? Also kernel command line you're using? Also what display are you using?

 

Kernel parameters change sometimes between two BSP releases, so make sure you're using correct parameters for your setup.

0 Kudos
Reply